This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In debugging DMS, the deserializer registers are configured as follows, but it does not work. I wonder if I need to configure registers for the serializer, Can you help provide the demo code of the driver?
{0xb3, 0x89},
/*Controls the CSI Transmitter frequency 800Mbps*/
{0x1f, 0x02},
/*Port 0 Receiver Enable, Port 1 Receiver Enable*/
{0x0c, 0xbf},
/*SETUP PORT SEL RX0*/
{0x4c,0x12},
/*FPD-Link III Input Mode RX0: RAW10 Mode/100 MHz */
{0x6d,0x7c},
/*config back channel*/
{0x58,0x5e},
//{0x5C,0xB0, 0xff, 1},
/*Internal Generated FrameSync*/
//{0x19,0x0A, 0xff, 1},
//{0x1A,0xD7, 0xff, 1},
//{0x1B,0x61, 0xff, 1},
//{0x1C,0xA0, 0xff, 1},
{0x18, 0x01},
/*RAW10 Mode Virtual Channel
This field configures the CSI Virtual Channel assigned to the
port when receiving RAW10 data.*/
{0x70,0xed},
/*Mapping Virtual Channel ID 0 to Port 0*/
{0x72,0xe8},
/*RX0 Normal RAW10, truncate frames, LV,FV polarity low*/
{0x7c,0x01},
/*setup csi 4 lane ,Enable CSI output */
{0x33, 0x01},
/*basic synchronized forwarding*/
{0x21, 0x3c},
/*disable RX port 1 forwarding*/
{0x20,0x20}
重复了。有什么问题我会在上述链接中跟进。所以这个帖子我暂时就先关闭了。