Part Number: DS90UB936-Q1
-
In debugging DMS, the deserializer registers are configured as follows, but it does not work. I wonder if I need to configure registers for the serializer, Can you help provide the demo code of the driver?
-
{0xb3, 0x89},
/*Controls the CSI Transmitter frequency 800Mbps*/
{0x1f, 0x02},
/*Port 0 Receiver Enable, Port 1 Receiver Enable*/
{0x0c, 0xbf},
/*SETUP PORT SEL RX0*/
{0x4c,0x12},
/*FPD-Link III Input Mode RX0: RAW10 Mode/100 MHz */
{0x6d,0x7c},
/*config back channel*/
{0x58,0x5e},
//{0x5C,0xB0, 0xff, 1},
/*Internal Generated FrameSync*/
//{0x19,0x0A, 0xff, 1},
//{0x1A,0xD7, 0xff, 1},
//{0x1B,0x61, 0xff, 1},
//{0x1C,0xA0, 0xff, 1},
{0x18, 0x01},/*RAW10 Mode Virtual Channel
This field configures the CSI Virtual Channel assigned to the
port when receiving RAW10 data.*/
{0x70,0xed},
/*Mapping Virtual Channel ID 0 to Port 0*/
{0x72,0xe8},
/*RX0 Normal RAW10, truncate frames, LV,FV polarity low*/
{0x7c,0x01},
/*setup csi 4 lane ,Enable CSI output */
{0x33, 0x01},
/*basic synchronized forwarding*/
{0x21, 0x3c},
/*disable RX port 1 forwarding*/
{0x20,0x20}