This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,UB936支持电压和温度测量。可以通过配置温度上下限阈值来触发内部温度传感器,当温度低于下限或高于上限值时会触发alarm信号,具体可以参考Table7-31~7-36的寄存器配置。
寄存器0x5A的状态可以知道是否已经触发内部温度传感器。
HI Kallyn
我们目前的情况是没有配置温度传感器的阈值,未使用此功能,当温度超过105℃会不会对935造成损坏
您好,105度您指的是环境温度吧?因为UB935的操作温度范围为-40~105度。
如果低于-40度或高于105度都不能保证芯片的电气性能,也就是说数据手册中的电气参数都不能保证。
也不能保证它的长期工作。