Part Number: DP83848Q-Q1


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请看如下答复:
以下是在 DP83848上运行 BIST 的步骤:
1. 通过将 BMCR 寄存器的环回位设置为1来启用环回模式
2. (optional)将 PHYCR 中的 PSR_15位设置为使用15位伪随机序列、,而不是默认的9位序列
3. 通过将 PHYCR 寄存器的 BIST_START 位设置为1来启动 BIST
4. 通过读取 PHYCR 的 BIST_STATUS 位来读取结果,以检查它是1 (通过)还是0 (失败)
同样对于100M 运行,BMCR 值也将是0x6100。