This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848Q-Q1: 如何操作用BIST验证DP83848Q的发送链路与接收链路的完整性(基于100m/s数据流)

Part Number: DP83848Q-Q1


  • 您好,您的问题我们需要升级到英文论坛寻求帮助,如有答复将尽快回复您。

  • 您好,请看如下答复:

    以下是在 DP83848上运行 BIST 的步骤:

    1. 通过将 BMCR 寄存器的环回位设置为1来启用环回模式

    2. (optional)将 PHYCR 中的 PSR_15位设置为使用15位伪随机序列、,而不是默认的9位序列

    3. 通过将 PHYCR 寄存器的 BIST_START 位设置为1来启动 BIST

    4. 通过读取 PHYCR 的 BIST_STATUS 位来读取结果,以检查它是1 (通过)还是0 (失败)

    同样对于100M 运行,BMCR 值也将是0x6100。