This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913/914调试问题

请求各位IT大神,小弟正在调试913/914的板子,自己做的

 

目前没有通,913时钟设置为image clk,我的sensor输出是48M的时钟,目前lvds好像没通,无法在914上输出图像

 

914的clk,hs,vs,data管脚都是输出一个780hz左右的窄脉冲,如图所示

 

913的i2c读写正常,可以访问913的寄存器,

914的i2c接口不能访问

lvds管脚上的信号大概是如下波形

请求大神给我指导一下,问题可能在哪儿,应该查一下哪块地方。

  • 自己回一个。

    继续测试,把913的寄存器都读出来看了看,大部分寄存器都是默认状态或者正确的状态。

    但是0xc 寄存器,读出来数字是0x24,最后一位是0,按照pdf的解释是   cable link not detected。我的913和914的lvds信号,没有按照demo板上加滤波电感,就是913的信号出来靠近芯片串0.1uF电感,然后再914靠近芯片的地方串0.1uF电感,这样会有问题么。