This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于04806双PLL输出时钟有50hz干扰非常疑难问题,请教

目前用了个04806,双PLL模式,参考时钟是FPGA从cpri口恢复四分频得到30.72MHz,vctcxo是30.72Mhz,输出为122.88MHz及其倍频分频时钟。

现在的现象是:

1. FPGA恢复的30.72MHz中心频点两边+/-50hz处有较大干扰(-40db左右)

2. vctxco输出30.72mhz同样有一定的50hz对称干扰(-60db左右)

3. 此时输出时钟中心频点两边+/-50hz,干扰会很大(-30db左右),杂撒相位噪声 也很严重,严重影响RF发射信号。

4. 如果cpri口仅仅保持link,而发数据为全0时,则FPGA内部相应模块不工作(不走数据),则恢复出的30.72MHz的50Hz干扰非常小。04806输出时钟也会特别好(无杂撒噪声,50hz干扰也很小)。

有人遇见过么?  提两个问题

1. FPGA逻辑多启用一点,怎么会引发恢复时钟50hz干扰的有无?(FPGA电流供应充足,其他逻辑都删掉,仅保持cpri口时钟恢复模块,也不能改善)

2. 04806双锁相环,参考钟和vctcxo输出都有50hz干扰的情况下,我可以将loop2 的环路带宽尽量改小,已压制第一级锁相环输出时钟杂撒干扰,尽量保持04806内部vco输出时钟的质量吗? 这样做,锁相环仅仅锁定时间变长,稳定性会变差吗?