Now can normal figure, but will appear some frame error, cause the mipi received frame num do not match. After these frames, can also be normal figure.
can you give some advices?
sensor: 2592 1944, 30fps 4lane
here is the 954 setting:
0x0c, 0x81
0x1f, 0x02
0x4c, 0x01
0x0a, 0x06,
0x0b, 0x0c
0x4a, 0x10
0xba, 0x00
0x0f, 0x3f
0x15, 0x41
0x16, 0x61
0x6f, 0x32
0x5c, 0x30
0x58, 0x5e
0x5d, 0x6c
0x65, 0x62
0x6d, 0x7c
0x72, 0xe4
0x33, 0x03
0x20, 0x20
953 setting:
0x0b, 0x20
0xff, 0x0a
0x0e, 0xF0
0xff, 0x0a
0x0d, 0xc0
0x0d, 0xc1
0x0d, 0xc3
0x0b, 0x06
0x0c, 0x0b
0x02, 0x73
0x06, 0x43
0x07, 0x7D
0xff, 0x0a