This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041-Q1 能设计成7个USB3.0 port吗

Other Parts Discussed in Thread: TUSB8041-Q1, TUSB8041EVM, TUSB8041

TI专家, 您好

         TUSB8041-Q1是一个四端口USB3.0 hub控制器。目前我们需要一个7端口的USB3.0 hub, 请问TUSB8041-Q1可以通过级联或其他方式支持7个端口的USB3.0吗?另外TUSB8041-Q1的驱动支持WIN8系统吗?

        期待您的回复!谢谢~

  • 可以级联的,参考它的应用框图

  • 关于可支持的操作系统,在datasheet中也有描述:

    No Special Driver Requirements; Works Seamlessly on any Operating System with Stack Support。

  • 非常感谢Kailyn~

    评估板地址: http://www.ti.com/tool/tusb8041evm

    TI有一个TUSB8041的评估板,4个USB3.0端口,如果要达到7个USB3.0端口,就是按下图连线就可以了,对吧???另外还有两个问题需要确认下:

    (1)用TUSB8041,需不需要用户写驱动程序呢?按我的理解,是不需要的,按照评估板的设计应该直接可以用(有疑惑的是看到评估板原理图有DOWNSTREAM PORT POWER SWITCHES电路,这些使能信号应该是TUSB8041芯片根据检测到USB有连接自动发信号的)。只是想确认下。

    (2)这种级联的设计,对后面USB4,5,6,7端口的速度没什么大的影响吧?

  • 1)不需要写驱动程序。

    2)USB4,5,6,7的速度就看上行端口的速度,换句话说,就看PC的速度是支持USB 高速,全速还是低速。

    When the upstream port is connected to an electrical environment that only supports high-speed or full-speed/low-speed connections, SuperSpeed  USB connectivity is disabled on the downstream ports. When the upstream port is connected to an electrical environment that only supports fullspeed/
    low-speed connections, SuperSpeed USB and high-speed connectivity are disabled on the downstream ports.

x 出现错误。请重试或与管理员联系。