Hello experts!
Could you tell me the chip TCAN1044V-Q1, which behaves the same in normal mode when receiving WUP as it does in standby mode? Will it pull down the RX pin?

thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello experts!
Could you tell me the chip TCAN1044V-Q1, which behaves the same in normal mode when receiving WUP as it does in standby mode? Will it pull down the RX pin?

thanks!
您好,我们可以直接使用中文沟通。
您的意思是normal mode下,当收到WUP之后,RX会拉低吗,是这个意思吗?
事实上,WUP指的是wake-up pattern。那只有在当standby mode下,才会收到WUP唤醒pattern,从standy 到normal 转换的一个过程。
接收到WUP之后,STB由high 到low转换,本地CAN协议控制器监测RXD由高到低转换从而重新激活device进入到normal mode。
不知是否能解决您的问题。有问题再讨论。
TCAN1044也是支持远程唤醒remote wake的,是通过WUP来支持远程唤醒的。
您说的通过TX,RX两根信号线是如何实现远程唤醒的?
可以参考数据手册9.4.6.1 Remote Wake Request via Wake Up Pattern (WUP)部分的介绍。