This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1044V-Q1: Normal mode Will it pull down the RX pin when receiving WUP?

Part Number: TCAN1044V-Q1


Hello experts!

 

Could you tell me the chip TCAN1044V-Q1, which behaves the same in normal mode when receiving WUP  as it does in standby mode? Will it pull down the RX pin?

thanks!

  • 您好,我们可以直接使用中文沟通。

    您的意思是normal mode下,当收到WUP之后,RX会拉低吗,是这个意思吗?

    事实上,WUP指的是wake-up pattern。那只有在当standby mode下,才会收到WUP唤醒pattern,从standy 到normal 转换的一个过程。

    接收到WUP之后,STB由high 到low转换,本地CAN协议控制器监测RXD由高到低转换从而重新激活device进入到normal mode。

    不知是否能解决您的问题。有问题再讨论。

  • 您好!

    1.在CAN协议里面是没有STB引脚的,我是否可以不用这个引脚,仅使用RX引脚来进行远程唤醒?

    2.如此该芯片不支持,是否有支持远程唤醒的仅TX RX两根信号线的芯片推荐?

    谢谢!

  • TCAN1044也是支持远程唤醒remote wake的,是通过WUP来支持远程唤醒的。

    您说的通过TX,RX两根信号线是如何实现远程唤醒的?

    可以参考数据手册9.4.6.1 Remote Wake Request via Wake Up Pattern (WUP)部分的介绍。

    https://www.ti.com/lit/ds/symlink/tcan1043h-q1.pdf