This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LV1023A: SN65LV1023+SN65LV1224

Part Number: SN65LV1023A
Other Parts Discussed in Thread: SN65LV1224B,

We designed a serdes function with SN65LV1023A and SNLV1224B, each chip supplier with separate power supply and clock, the link between the serdes is only twisted/shielded LVDS cable, no other signal. The question is we found that the SN65LV1224B never locked, and note that the input to the serializer not always with data, some times some channels are always high or always low and rest channels with data. Could you help to check the design below, and give your comments, thanks in advance!

  

  • The layout has a separate analog and digital ground, all the serializer and deserializer data input and LVDS output are impedance matched and with same length, schematic as below.

  • and note that the input to the serializer not always with data, some times some channels are always high or always low and rest channels with data

    这里指的输入给1023A的数据不总是数据,有时候的总是高电平或低电平,其余的通道是data,这里是什么意思?

    另外,电路中SYNC1通过两个10K电阻分压之后为1/2*VCC=1.65V ,即不是高电平也不是低电平,TTL输入的Vih(min)=2V,所以您是想使用下列哪种同步方式?

  • 不总是有数据,是说有些输入在一段时间内可能是没有高低电平变化的,比如片选的CS,会持续为高,或者持续为低。

    SYNC1的两个电阻是预留位,实际上,仅通过一个0欧电阻接到GND的。另外,TCLK_R/F#以及RCLK_R/F#均为0欧电阻短接到GND。

    目前采用的是random lock的方式。

  • sync 1和sync2是通过或门连接的,所以建议是至少其中一个为高电平,启动同步模式,这样的话能够更快的建立同步时序,在编解码过程中能找到pattern的start/end边界保持同步。

    不总是有数据,是说有些输入在一段时间内可能是没有高低电平变化的,比如片选的CS,会持续为高,或者持续为低。

    另外不能锁存的原因和输入有关,就是根据您的输入来看,直接DC耦合到输入端的是吧?很有可能是因为DC 不平衡导致,位流中出现多个连续的1或者0会导致编码错误。

    您可以尝试输入1和0交替出现的输入信号试下,输出是否能lock。

  • 但是我们的设计有个问题是方案不带MCU,仅加串解串功能,我会尝试用解串的LOCK信号接到加串SYNC1在测试一下。但是实际应用中,由于解串与加串间会有3到5米的线缆,lock信号的传递需要增加额外成本,所以我们希望能直接用random lock的方式。对于以上需求,以及电路,烦请帮忙看一下有没有可以改进的地方,包括电路上的,谢谢!

  • 没有MCU,可以直接给sync一个高电平试试。

    但是我认为没有lock的更大的原因是因为输入的位流中出现多个连续的1或者0会导致编码错误。

    电路我看了下,就是模拟地和数字地我看都是接在一起的,那么在layout中建议是分开,可以用磁珠连接。