Other Parts Discussed in Thread: SN74CBTD3861, SN74CBTLV3861, SN74LVC8T245, SN74LVC16T245, TXB0108
请问一下,SN74CBTD3861这个芯片3.3V和5V可以互转吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74CBTD3861, SN74CBTLV3861, SN74LVC8T245, SN74LVC16T245, TXB0108
请问一下,SN74CBTD3861这个芯片3.3V和5V可以互转吗
TI 的CBT和CBTD系列的逻辑产品中,如果是5VCMOS电平,那么只能实现5V CMOS到3.3V的单向转换,如果是5V TTL电平的话,可以实现5V TTL和3.3V的双向电平转换。
另外,补充一下,为什么可以实现5V TTL到3.3V双向电平转换,是因为5V TTL电平和3.3V LVTTL电平的阈值电平是一致的(Vih,Vil,Voh,Vol).
有一个600k左右的脉冲信号,其高电平是3.3V ,现在想把它高电平抬高到5v 用SN74CBTD3861这个芯片能实现吗
麻烦再问下,SN74CB3861DW可以实现将3.3V的脉冲信号转成5V的脉冲信号吗
没有SN74CB3861这个型号啊,是不是SN74CBTLV3861?
SN74CBTD3861DW不就是你一开始问的SN74CBTD3861这款器件吗?二者是同一款器件哦,后缀DW指的是SOIC的封装。
之前已经回复,如果是5V TTL的话,可以实现双向电平转换,看你目前的意思是想要抬高5V,应该是5V CMOS电平,SN74CBTD3861这款不可以的呢。 你是几路信号啊? 来帮选一款3.3V到5V的器件。
嗯 是的 我想问的是这个芯片能将3.3V的脉冲信号转到5V吗
是的 就是将3.3v的脉冲信号 抬高到5V,是10路的 能推荐一下哪款芯片能实现吗 8路以及其它路的也行 谢谢!!!!
8路或者16路的常见,比如常用的8路的LVC系列的,SN74LVC8T245,16路的SN74LVC16T245.都可以实现3.3V到5V的双向电平转换,不过都是双电源供电的,不知是否满足你的要求,另外脉冲信号的频率为多大?
8路和16路的都可以 我的脉冲信号大概是3.3V 的700kHZ的 能转到5V不?
8路和16路的都可以 我的脉冲信号大概是3.3V 的700kHZ的 能转到5V不? 另外能否推荐一款5V和3.3V脉冲信号互转的芯片 谢谢!!!
8路的双电源转换芯片TXB0108你看看行不行,不过这个需要两组电源
可以,700KHz没问题。zhong yuan xu 说:8路和16路的都可以 我的脉冲信号大概是3.3V 的700kHZ的 能转到5V不?
能否推荐一款5V和3.3V脉冲信号可以互转的芯片型号 谢谢!!!
我刚说的SN74LVC8T245和carter说的TXBxx的都是3.3V和5V双向转换的哈,不是单向的,只是这两种都是双电压供电的,不知是否满足你的要求。
谢谢 可否推荐一款单电源的将3.3V脉冲信号转5V的芯片型号?
太感谢了 可否再推荐一款单电源的将3.3V脉冲信号转5V的芯片型号?
单电源转换不能满足你的多路要求,单电源的都是1路的。