This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问一下,SN74CBTD3861这个芯片3.3V和5V可以互转吗
TI 的CBT和CBTD系列的逻辑产品中,如果是5VCMOS电平,那么只能实现5V CMOS到3.3V的单向转换,如果是5V TTL电平的话,可以实现5V TTL和3.3V的双向电平转换。
另外,补充一下,为什么可以实现5V TTL到3.3V双向电平转换,是因为5V TTL电平和3.3V LVTTL电平的阈值电平是一致的(Vih,Vil,Voh,Vol).
有一个600k左右的脉冲信号,其高电平是3.3V ,现在想把它高电平抬高到5v 用SN74CBTD3861这个芯片能实现吗
麻烦再问下,SN74CB3861DW可以实现将3.3V的脉冲信号转成5V的脉冲信号吗
没有SN74CB3861这个型号啊,是不是SN74CBTLV3861?
SN74CBTD3861DW不就是你一开始问的SN74CBTD3861这款器件吗?二者是同一款器件哦,后缀DW指的是SOIC的封装。
之前已经回复,如果是5V TTL的话,可以实现双向电平转换,看你目前的意思是想要抬高5V,应该是5V CMOS电平,SN74CBTD3861这款不可以的呢。 你是几路信号啊? 来帮选一款3.3V到5V的器件。
嗯 是的 我想问的是这个芯片能将3.3V的脉冲信号转到5V吗
8路或者16路的常见,比如常用的8路的LVC系列的,SN74LVC8T245,16路的SN74LVC16T245.都可以实现3.3V到5V的双向电平转换,不过都是双电源供电的,不知是否满足你的要求,另外脉冲信号的频率为多大?
我刚说的SN74LVC8T245和carter说的TXBxx的都是3.3V和5V双向转换的哈,不是单向的,只是这两种都是双电压供电的,不知是否满足你的要求。