This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CDCE913的问题

Other Parts Discussed in Thread: CDCE913

TI工程师,你好:

        这封邮件打扰你了,请教关于CDCE913的问题:

1、VDD的供电电压是1.8V,SCL和SDA的接口电平3.3V这样可以工作吗,是否需要转换成一样的?

2、如果上面的问题,接口电平3.3V可以工作的情况下,在对CDCE913进行寄存器设置时,发现数据设置不进去,不管哪个寄存器读回来都是0x07,我写操作是这样的流程:

先写0x02~0x06的寄存数据,再写0x10~0x1F的寄存数据,然后再写:0x06中的EEWRITE位,寄存器值是0x41,写完后,延时100ms,去读取EEPIP位是否编程完成,完成后,再写把数据lock进来。

不知道我这样流程对不对,希望能得你们的帮助,谢谢

在线等待中。。。

CDCE913

x 出现错误。请重试或与管理员联系。