Part Number: DP83826I
用RJ45网线连接两台以太网设备, 正常状态下,两台以太网网口LED0黄灯闪烁,代表有数据交互。
但是偶尔出现以下情况
1.LED0黄灯不亮
2.LED1绿灯常亮
3.BMCR Register, BMSR Register, PHYIDR1 Register的值都是0xBBB5
这是什么情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LED0黄灯闪烁代表发送或接收端是active状态的,如果发送和接收都active的话,LED0应该是常亮。
LED0不亮,说明发送和接收都处于无效状态,可能link不稳定。
LED1常亮的话代表速率为100M, 如果不亮的话是10M或者no link。 那LED1常亮说明速率没问题。
从这两个寄存器来看的值,可以确认link是没问题的,配置的是100Mbps,在自动协商这里是无法执行的,两台以太网都使能了自动协商是吗?
您好,
同一块电路版上面的另一个正常工作的phy没有这种现象。
正常工作的PHY也是使用的DP83826吗?
两台以太网设备都是使用的DP83826是吧?只是有一片不能正常工作,是这样的吗?
是否有做交叉试验,看下是芯片的问题还是板子的问题?