您好,在win7 64位系统上使用TSBKS8000HCI评估板资料中的ti_echo.exe ti1394.exe ohcirom.exe软件时,无法打开这三个软件,并报错。双击软件图标,也是报错。如下图所示,请问正确打开这三个软件的方式是什么?在什么系统上可以使用这三个软件?谢谢您。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,1394的器件比较老了,这两个软件我记得XP系统是会报错的,WIN7好像是可以打开的,我去和美国工程师确认下。然后尽快给您答复。
您使用的ti_echo.exe ti1394.exe ohcirom.exe这两个有版本吗?
您好,关于您的问题,我这边收到回复如下:
I believe the SW is 32-bit only. Also, it may only assume a 32-bit PCI bus, but I thought 32-bit PCI devices would work on a 64-bit bus as well.