This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB984-Q1 eDP驱动屏幕

Other Parts Discussed in Thread: DS90UB984-Q1

DS90UB984-Q1 eDP输出给屏幕正常显示的时候,给屏幕重新断电再上电,有概率屏幕亮不起来(30%)

屏幕无法点亮时,给解串器0x60寄存器写0x01可以恢复正常显示

请问出现这种情况的原因?

  • 您好,

    我们正在联系内部其他同事的协助,需要一些时间来完成。请您耐心等待我们的通知。

  • 你是否做过这样的测试,即仅配置寄存器0x1 = 0x40?

    Has the customer tested only running 0x1 = 0x40 instead of 0x60?

    30%是指什么的概率?同一块板子循环上电的故障率还是产品的故障比率,即有30%的产品有这种现象?如果是指前一种,那产品的故障率是多少?