This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
将P7和P17配置为输入,电平变为低后,I2C时钟消失,如果是高,就不会有问题
您好,
是说SCL吗?这个管脚是主机控制的,芯片不会影响它。
请检查是否其他软件功能禁止了I2C通讯。
此I2C下挂了8个TCA9535从站,I2C总线未接电容,接10K上拉电阻,可以这样设计吗?
TCA9535有三个地址管脚,最多支持8个芯片在一个I2C总线上。
上拉电阻计算请参考下面文档。
I2C Bus Pull-Up Resistor Calculation
TCA9535能改变其上电默认电平状态吗?
不能,IO口上电默认是输入状态,请查看寄存器的上电 default值。
上电后,可通过寄存器配置更改。
如有新的问题,请重新发帖咨询。