This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.AUX_IN不用的话,VCC_AUX需要怎么处理?
2.该参数表示差分输入端口差分后的电压摆幅还是单臂电压摆幅范围?(通常differential input中的VIH,VIL参数都是表示单臂电压参数吧,对吗?)
4.输入端可接收LVPECL,LVDS,LVCMOS形式的信号,那一定频率的单载波信号可以作为输入吗?
VCC_AUX还是需要接上3.3V,因为这个不仅仅是crystal的供电,还是内部输入buffer模块的供电,所以即使不使用crystal输入,还是需要把3.3V接上。
4.你说的单载波信号频率多大?电压范围是多少,看下是否满足CDCE62005的输入要求,如果满足也是可以作为输入的。
考虑后,单载波还是需要转为差分
变压器转换后的信号:
VCM=900mV
VPP=615mV
输入频率为10MHz,输出频率为200M
请教下:
1.一般需要满足什么样的要求,单载波也能输入?
2.差分输入需要做阻抗匹配的话那差分输入阻抗是多少?差分输入模式那块只是提到了input capacitance为3pF
考虑后,单载波还是需要转为差分
变压器转换后的信号:
VCM=900mV
VPP=615mV
输入频率为10MHz,输出频率为200M
可以作为输入吗?
请教下:
1.一般需要满足什么样的要求,单载波也能输入?
2.差分输入需要做阻抗匹配的话那差分输入阻抗是多少?差分输入模式那块只是提到了input capacitance为3pF
单载波的话就是LVCMOS输入, LVCMOS输入的话,输入频率最高位250Mhz,输入要求Vih(min)=0.7Vcc,Vil(max)=0.3Vcc。