This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LVDS接口芯片DS90C363, DS90CF364

Other Parts Discussed in Thread: SN65LVDS96, DS90C363, SN65LVDS94

1、芯片内部PLL处理CLK信号,是否是进行倍频、降频处理,来保证CLK输入输出大小不变的?

2、DS90C363和SN65LVDS96配对使用,会出现失真,是不是必须得DS90C363/4搭配使用?

3、DS90C363可以和SN65LVDS94配对用吗?

请大神指点一下。

  • 1、芯片内部PLL处理CLK信号,是否是进行倍频、降频处理,来保证CLK输入输出大小不变的?

    A:是指的DS90C363这款内部PLL吗?不需要倍频,降频处理。

  • 2、DS90C363和SN65LVDS96配对使用,会出现失真,是不是必须得DS90C363/4搭配使用?

    A: DS90C363和SN65LVDS96搭配使用不合理,DS90C363是LVDS输出,而SN65lvds96是TTL输入,另外DS90C363/4是FPD link的应用,即使不适用DS90C364搭配使用,可以考虑SN65LVDS84这类搭配。

  • 3、DS90C363可以和SN65LVDS94配对用吗?

     A: DS90C363可以和SN65LVDS84配对使用。

  • Thank you,Kailyn Chen

  • 不客气,有问题大家可以再讨论。

  • 你好,给你推荐一个比较符合你要求的高速率传输芯片  THCV231/236  

    THCV231可以将最高12Bit/pixel的LVCMOS并行信号转换为串行图像信号的发送端IC。最其具备大传输速率3.2Gbps的CML串行输出,可以将1080p60Hz的12bit摄像头图像信号通过一对双绞线或者一根同轴电缆进行传输。此外,可以通过双向的传输通道进行I2C信号传输。

    THCV236/可以将THCV发送端IC输出的串行图像信号转换为最高32bit/pixel的LVCMOS并行图像信号的接受端IC。1080p60Hz的16bit的摄像头图像信号通过一对双绞线或者一根同轴电缆进行接收。此外,还具备一条可以用来传输I2C、UART或GPIO等串行信号的Sub-Link,向传输通道“Sub-Link"  I2C/UART/GPIO(最高4条)

    详细信息可看官网http://www.thine.co.jp/zh_cn/products/num_details/THCV231.html,我司可提供规格书、样片和技术支持,欢迎联系qq:2817821256 手机18682112448