This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A芯片输入8位数据电路应该如何接到输入端?

你好!TI 工 程师

请问,DS90UB913A芯片输入8位数据电路应该如何接到输入端?如果接法是对的,DS90UB913A芯片因为没有说明8BIT的工作模式,设置是采用10BIT还是12BIT的工作模式!

请支持,谢谢!

  • 8bit的话,使用DIN[0:7].

  • Dear Kailyn,

    是否一定要接到DIN(0-7)呢,如果913采用DIN(2-9), 同时在914端也是接到DIN(2-9),是否可行呢?谢谢!

    我目前用这种接法无法得到图像输出,附上我测试的913输入HS,VS,PCLK,FYI

    DS90UB913A input wave.rar
  • 不一定接到DIN(0-7),如果913采用DIN(2-9), 同时在914端也是接到DIN(2-9),这是允许的,因为914的输出是对应913的输入的。

  • Dear Kailyn 

    我们目前数据接口是没错的。我们的项目用于车载摄像头,采用了专用的ISP芯片输出数据,再送至DS90UB913A,

    目前测试ISP输出CLK, VS, HS及数据有输出,初步判断前端没问题,但913输出LVDS测试无任何信号输出,想请教如何判断Cable端输出的LVDS信号正常呢?

    附上我们DS90UB913A部分原理图供参考,谢谢!

    SI6-CB-V0.1-150915.pdf
  • 你好,给你推荐一个比较符合你要求的高速率传输芯片  THCV231/236 

    THCV231可以将最高12Bit/pixel的LVCMOS并行信号转换为串行图像信号的发送端IC。最其具备大传输速率3.2Gbps的CML串行输出,可以将1080p60Hz的12bit摄像头图像信号通过一对双绞线或者一根同轴电缆进行传输。此外,可以通过双向的传输通道进行I2C信号传输。

    THCV236/可以将THCV发送端IC输出的串行图像信号转换为最高32bit/pixel的LVCMOS并行图像信号的接受端IC。1080p60Hz的16bit的摄像头图像信号通过一对双绞线或者一根同轴电缆进行接收。此外,还具备一条可以用来传输I2C、UART或GPIO等串行信号的Sub-Link,向传输通道“Sub-Link"  I2C/UART/GPIO(最高4条)

    详细信息可看官网http://www.thine.co.jp/zh_cn/products/num_details/THCV231.html,我司可提供规格书、样片和技术支持,欢迎联系qq:2817821256 手机18682112448