This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB422: 评估SNK能力后,选择PDO,直接进入Hard Reset Rx'd,然后重置反复重启

Part Number: TUSB422


 ________  _________  ____ ___  ___
/_  __/ / / / __/ _ )/ / /|_  ||_  |
 / / / /_/ /\ \/ _  /_  _/ __// __/
/_/  \____/___/____/ /_//____/____/

PD Stack v1.03
=====================================
UNATTACHED_SNK
Port[0]: addr: 0x20, SNK, Rp: 3.0A, Flags: None.
VID: 0x0451
PID: 0x0422
DID: 0x0100
REV: 0x02
CC status = 0x13
ATTACH_WAIT_SNK
CC status = 0x13
CC status = 0x11
CC status = 0x13
ATTACHED_SNK
PE_SNK_STARTUP
Mux: USB
PE_SNK_DISCOVERY
PE_SNK_WAIT_FOR_CAPS
PD Rx
PE_SNK_EVALUATE_CAPABILITY
PDO-1 Fixed, 5000 - 5000 mV, 3000 mA, 15000 mW
PDO-2 Fixed, 9000 - 9000 mV, 3000 mA, 27000 mW
PDO-3 Fixed, 12000 - 12000 mV, 3000 mA, 36000 mW
PDO-4 Fixed, 15000 - 15000 mV, 3000 mA, 45000 mW
PDO-5 Fixed, 20000 - 20000 mV, 5000 mA, 100000 mW
PDO-2 0x0002d12c selected
PE_SNK_SELECT_CAPABILITY
Hard Reset Rx'd.
PE_SNK_TRANSITION_TO_DEFAULT
PE_SNK_STARTUP
PE_SNK_DISCOVERY
Mux: USB
PE_SNK_HARD_RESET
PE_SNK_TRANSITION_TO_DEFAULT
PE_SNK_STARTUP
PE_SNK_DISCOVERY
Mux: USB
Mux: USB
UNATTACHED_SNK
PE_UNATTACHED
Mux: Disable
CC status = 0x30
PE_SNK_HARD_RESET
PE_SNK_TRANSITION_TO_DEFAULT
PE_SNK_STARTUP
PE_SNK_DISCOVERY
UNATTACHED_SNK
PE_UNATTACHED
Mux: Disable
UNATTACHED_SNK
PE_UNATTACHED
Mux: Disable

电路连接如下

请问该调整哪里?谢谢。