This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DP159: 和xilinx的FPGA结合使用,内部由FPGA实现HDMI核

Part Number: SN65DP159


参考xilinx的ZCU102相关设计,但是FPGA使用K7系列,结合自己的应用,没有使用DDC,HDP_SNK信号在我的设计中直接上拉到了3.3V,使用XILINX的HDMI核输出分辨率为1080p@60Hz分辨率视频。

在调试中,DP159输入信号的AC耦合前后断信号都有信号(时钟频率正确,为148.5MHz,时钟单端摆幅约为200mv),并参照xilinx的demo程序进行了配置,且配置后读取的值与预想配置的值一致。

但是在DP159的后端没有对应的波形输出,通过排查,包括电源、OE、HPD等信号的状态,都满足要求,但是无论如何配置都无法输出。

更换了一个DP159后,现象完全一致。

在手册上我看到DP159处于低功耗模式只与OE和HPD_SNK状态相关,但是这两个信号也都正常,且芯片输入信号也正常。请问导致DP159无法输出的原因还有哪些?

请帮忙解答一下,非常感谢!