This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
下面是1MHZ以上的TCA9617B的类似功能型号,您可以在列表中package size一项中,查看芯片尺寸:
www.ti.com.cn/.../products.html
Dear Eirwen:
列表里面除了TCA9617B其他都是Voltage-Level Translator,请教下,是不是只有repeater 的A port Vol不受B port Vol影响,
Voltage-Level Translator的A port Vol受B port Vol影响?
因为不能确定B port端的device型号和数量。
谢谢!
Voltage-Level Translator的A port Vol可以参考数据表,例如TCA9617B数据表6.5 Electrical Characteristics的VOLA,MAX是0.4V, 不受受B port Vol影响。
TCA9617B不是Voltage-Level Translator,是 Repeater,repeater 的A port Vol不受B port Vol影响。
Voltage-Level Translator的A port Vol受B port Vol影响吗?
比如,TCA9409,VolA max0.4V,但是我不确定VolA <0.4V时,是否对B port端有要求,比如上拉电阻和漏电流。
帮忙看下,谢谢!
是的,按照TEST CONDITIONS,需要VIB小于015V时,可以满足VolA max0.4V