This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS100BR111: 背板CPU间连接使用DS100BR111,KR出现链路没有稳定

Part Number: DS100BR111


您好

  机箱中2块板卡通过机箱背板互连,背板走线长度>25inch; 为了改善CPU卡互连的USXGMII接口信号,每块板卡上都添加了DS100BR111芯片。使用KR pin模式调整,CPU两端使用iperf3 跑流量出现CPU

的USXGMII接口有很多错包;而后使用iic 模式进行配置调试;配置如图中所示;

0x6 0x18
0x8 0x04
0xf 0x00
0x10 0xad
0x11 0x00
0x16 0x02
0x17 0xad
0x18 0x00
0x23 0x00
0x28 0x00
0x2d 0x18

我调整A的EQ,大于2的时候接口便不通了;B的VOD 1300mv会情况会好些,单出现的fcs 仍会有十万分之一;

请问下:

这样连接的时候,配置情况感觉信号强度高了,是否有方法确认吗?

CPU端 USXGMII接口与其他交换连接,情况正常,测试接口无错包的。

感谢