This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB983-Q1: 983 + 948 REM_INT中断

Part Number: DS90UB983-Q1


我用983驱动948的中控屏幕,测试画面都可以点亮,使用REM_INT接收TP的中断信号,TP是每10mS发送一次终端,但是我在983端监控间隔是100mS发送一次,我用949驱动中断是正常的,这个和什么寄存器有关系

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好,

    与983 SER 的 REM_INTB 功能相关的寄存器如下:

            ser.board.WriteI2C(ser.devAddr, 0xC6, 0x21)
            ser.board.WriteI2C(ser.devAddr, 0x1B, 0x88)
            ser.board.WriteI2C(ser.devAddr, 0x51, 0x87)
            ser.board.ReadI2C(ser.devAddr, 0x52)
    通过983上的这些寄存器启用该功能、回读可能发生在0x52上。

    这样、输出也应该在 GPIO4上作为输出进行传播。

    请告诉我这是否也是端口0、如果改为端口1、可能需要一些额外配置。