我用983驱动948的中控屏幕,测试画面都可以点亮,使用REM_INT接收TP的中断信号,TP是每10mS发送一次终端,但是我在983端监控间隔是100mS发送一次,我用949驱动中断是正常的,这个和什么寄存器有关系
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用983驱动948的中控屏幕,测试画面都可以点亮,使用REM_INT接收TP的中断信号,TP是每10mS发送一次终端,但是我在983端监控间隔是100mS发送一次,我用949驱动中断是正常的,这个和什么寄存器有关系
您好,
与983 SER 的 REM_INTB 功能相关的寄存器如下:
ser.board.WriteI2C(ser.devAddr,
0xC6
,
0x21
)
ser.board.WriteI2C(ser.devAddr,
0x1B
,
0x88
)
ser.board.WriteI2C(ser.devAddr,
0x51
,
0x87
)
ser.board.ReadI2C(ser.devAddr,
0x52
)
这样、输出也应该在 GPIO4上作为输出进行传播。
请告诉我这是否也是端口0、如果改为端口1、可能需要一些额外配置。