Part Number: DS90LV011A
Other Parts Discussed in Thread: SN74HCS126-Q1,
1、电路图如下,两个芯片互联,对应芯片型号分别为DS90LV011ATMFX和SN74HCS126PW-Q1
2、当我把电阻R55040的阻值由33欧姆调整成0欧姆,两个芯片的供电电源P3V3_MCU就会发生芯片短路,而且更换回33欧姆,还是对地短路
3、这两个芯片不能直接互联么,具体可能什么原因导致电源对地短路?
- Circuit Diagram: The two chips are interconnected, with model numbers DS90LV011ATMFX and SN74HCS126PW-Q1, respectively.
- Issue Description: When I adjust the resistance of resistor R55040 from 33Ω to 0Ω, the power supply P3V3_MCU for both chips becomes short-circuited to ground at the chip level. Even after reverting to 33Ω, the short circuit to ground persists.
- Question: Can these two chips not be directly interconnected? What specific reasons might cause the power supply to short-circuit to ground?