Part Number: SN75LVPE3410
1、Communication between XILINX KU060 and X86 is conducted via PCIE. Due to the long layout routing, buffer(SN75LVPE3410) is adopted for enhanced driving
2、Due to the excessive length of the wiring harness, two SN75LVPE3410s were added in the middle of the link

3、the settings of the buffer are as shown in the above figure.The result is that the PCIE bandwidth is reduced from X4 to X1
I want to know if there is anything wrong with this design!