• DS90UH983-Q1: MST未能显示

    Part Number: DS90UH983-Q1
    Other Parts Discussed in Thread: ALP

    您好:

           我们需要使用983的MST功能。但目前遇到link address failed 的问题,LINK_ADDRESS请求是DP协议规范中定义的,属于sideband message消息;在数据手册中有看到需要绕过边带消息和拓扑发现。如果需要绕过这些,如何进行allocate payload的操作,这也属于sideband message消息。我试着进行allocate…

  • DS90UB947-Q1: DS90UB947配置ALP链接问题

    Part Number: DS90UB947-Q1
    Other Parts Discussed in Thread: ALP

    您好!

    DS90UB948端是1920*720的液晶屏,我如何用DS90UB947来驱动显示?寄存器要如何配置?请指导一下谢谢!947硬件没有问题可以驱动1280*720的屏幕,还有就是ALP为什么链接不成功?求解

  • DS90UB988-Q1: DS90UB688RURRQ1 EOM

    Part Number: DS90UB988-Q1
    Other Parts Discussed in Thread: ALP, USB2ANY

    如何使用EOM监测 DS90UB688-Q1 FPD IV 的眼图

  • DS90UB962-Q1: FPD LINK眼图仿真

    Part Number: DS90UB962-Q1
    Other Parts Discussed in Thread: ALP

    我在官网上下载了DS90UB962-Q1的IBIS模型,想仿真眼图,但是没有AMI模型,请问仿真的时候均衡的参数怎么调呢

  • DS90UB935-Q1: FPD LINK接口上单端信号电压值如何降低?这个电压值过高是否会对EMI辐射发射有影响?

    Part Number: DS90UB935-Q1

    我们使用DS90UB935串行器设计的摄像头模组,测量接口上的单端信号电压值约1.1V,但看935的规格书这个单端信号电压最大应该为670mVp-p,请问是什么原因造成我们模组这个单端电压值过大,怎么降低这个单端电压幅值?这个电压值过高是否会对EMI辐射发射有影响?

    我司模组实测单端电压值:

    935手册单端电压值描述:

  • DS90UB948-Q1: DS90UB948-Q1: IIC 设置的地址与寻到的地址不匹配

    Part Number: DS90UB948-Q1
    Other Parts Discussed in Thread: ALP

    您好:

           现在我们客户端有个产品显示屏出现黑屏,解串器型号:DS90UB948-Q1。加串器型号:DS90UB941-Q1。经过查看LOG分析出,主机端SOC读取到的IIC地址为0x3f,然而我们实际项目中硬件设置的是0x34

     (电阻采用1%精度)。

    以下是规格书中IIC的地址,并没有0x3f这个地址。

    以下我们排查情况:

    1、我们已经把948端的上电时序排查了,跟规格书要求的一致…

  • DS90UB983-Q1: 安装ALP-PROFILE-UPDATE包,但没有UB983的profile

    Part Number: DS90UB983-Q1
    Other Parts Discussed in Thread: ALP

    安装了ALP后又ALP_PROFILE_UPDATE_v14_setup_v_1_57_0010,但ALP工具的可选设备里没有983,看了一下工具里profile,没有983的profile,98x系列的都没有profile

  • ALP配置DS90UB688

    Other Parts Discussed in Thread: ALP

    在ALP中是否可以通过“98x Script Gen Tool v5.5”脚本工具来配置DS90UB688-Q1?

  • DS90UB988-Q1: ALP配置DS90UB988

    Part Number: DS90UB988-Q1
    Other Parts Discussed in Thread: ALP

    在ALP中是否可以通过“98x Script Gen Tool v5.5”脚本工具来配置DS90UB988?

  • DS90UB981-Q1: 信号完整性测试

    Part Number: DS90UB981-Q1

    Hi E2E,

    我们想知道FPD-LINK的信号完整性测试,是不在屏解串器那端有两个专门pin脚供测试?有没有相关的方法介绍?

    同时是否有反向控制信号干扰的,是哪几个pin脚呢?

    BR

  • DS90UB948-Q1: DS90UB947和UB948相连,使用947内部图形生成器,为什么运行后947和948的Pixel Clock不一致

    Part Number: DS90UB948-Q1
    Other Parts Discussed in Thread: ALP

    第一张图是947内部图形配置,第二张图是像素时钟。947的像素时钟计算是对的,如下:

    2084*736*65.2=100,005,324,即100M。但是948的显示为85.965M。

    问题1:

    948的视频来源是947,那么它们的像素时钟不应该一样么?

    问题2:

    948的85.965M怎么计算得来的,是否有公式?

    问题3:

    实际测试UB948输出的LVDS时钟约46MHz…

  • DS90UB954-Q1: 不能出图

    Part Number: DS90UB954-Q1
    Other Parts Discussed in Thread: ALP

    高通845 linux,OX03C10 + DS90UB953 + DS90UB954。直接连接03C10可以正常使用。连接954、953后报 SOF Freeze。954和953配置如下。

    int main(int argc, char *argv[]) { if (Hardware::PC()) { printf("exiting, camerad…

  • DS90UB988-Q1: 参考官方的ALP工具生成的配置,988没有收到任何数据

    Part Number: DS90UB988-Q1
    Other Parts Discussed in Thread: ALP

    我在使用DS90UB981 and DS90UB988的时候,发现988没有收到任何数据,使用的配置是官方的ALP工具生成的配置。

    我通过查看988的page18 FPD RX link layer reg,0x36/0x37 packet_cnt,发现一直为0。

  • DS90UB924-Q1: 寄存器配置脚本

    Part Number: DS90UB924-Q1
    Other Parts Discussed in Thread: DS90UB983-Q1

    Hello, This is from Continental Automotive Interior system (Wuhu). Now we have one HUD product, which used DS90UB924-Q1 De-serializer. 

    Now, we need TI technical support to propose 

  • DS90UB953-Q1EVM: DS90UB953-Q1EVM可以不搭配DS90UB954-Q1使用吗

    Part Number: DS90UB953-Q1EVM
    Other Parts Discussed in Thread: DS90UB954-Q1, ALP

    嗨,大家好

    现在有一块DS90UB953-Q1EVM,可以直接用它发射信号连接示波器看眼图吗? 如果可以,它的符号速率可以更改吗?

  • DS90UH929-Q1: DS90UH929 IIC寄存器写入的问题

    Part Number: DS90UH929-Q1
    Other Parts Discussed in Thread: ALP

    您好,我用ALP怎么对0X66地址的器件写入address为0X66 data为0x02,0x32,0xbc   和data为0x01,0x01,0x00,0xff   ,ALP函数里没有找到相关的函数,只有board.WriteI2C(devAddr, regIndex, regVal)的函数,请问如何操作?谢谢! 

  • DS90UB983-Q1MEVM: Need ALP Profile

    Part Number: DS90UB983-Q1MEVM
    Other Parts Discussed in Thread: ALP

    Hi TI,

    I need the ALP profile to use this EVM in my design and am highly appreciated if you could point me to where to download it or send me it via mail. Thanks.

  • DS90UH949-Q1EVM: Cannot be Recognized in ALP Correctly As DS90UH949 but As DS90UH925

    Part Number: DS90UH949-Q1EVM
    Other Parts Discussed in Thread: ALP, USB2ANY, DS90UB925Q-Q1, DS90UB927Q-Q1, DS90UB928Q-Q1, DS90UH940-Q1, DS90UH948-Q1, DS90UH949-Q1

    As the picture shown below, my DS90UH949EVM board is not recognized correctly by ALP. On the…

  • DS90UB981-Q1: 使用ALP工具生成寄存器,导入后pattern可以正常出,dsi信号正常,但是不出图

    Part Number: DS90UB981-Q1
    Other Parts Discussed in Thread: ALP

    1、DSI0输入,使用vp0,single port0输出,对端948没做控制,DSI是1080P的信号,因为FDP3单port带宽不够,降帧到30fps
    2、根据ALP工具配置981寄存器,从981打pattern可以正常出图。
    3、DPHY_STATUS的状态是全F,DPHY其他状态ERR寄存器都是正常,但是VP_STS_VP0为全0,无图像输出,948双路输出无数据信号

  • DS90UB983-Q1EVM: DS90Ux983-Q1EVM开发板如何切换MCU与983的I2C接口

    Part Number: DS90UB983-Q1EVM
    Other Parts Discussed in Thread: USB2ANY, ALP

    你好!

    我们的983开发板使用发现,电脑无法识别983的设备信息,可能调试中损坏,MCU430和983之间有三组I2C接口,默认的是I2C0吗?能否切换到I2C1或者2上?是跳线帽直接跳过去就行还是MCU固件需要更改?

    请帮忙解答,多谢!

  • ALP: DS90UB983 使用SST模式如何正确生成输入的superframe尺寸

    Part Number: ALP

    使用串行器DS90UB983带动两个硬件屏幕,串行器采用SST模式输出superframe帧,VP0---屏幕1,VP1---屏幕2

    使用官方提供的ALP工具,在生成superframe时,出现报错,无法生成的情况

  • DS90UB953A-Q1: USB3ANY连接问题

    Part Number: DS90UB953A-Q1
    Other Parts Discussed in Thread: TDA4VM, USB2ANY, ALP, DS90UB954-Q1EVM

    您好,我们目前正在打算使用ds90ub953、ds90ub954和TDA4VM使用serdes通路,但是目前ds90ub953暂未获取。

    因此我们打算使用ds90ub954中的pattern generator生成图形模拟输入信号。现有两个问题想明确:

    1.我们目前将ds90ub954供电,并将其与TDA4VM相连…

  • ALP: 执行board.WriteI2C,报错AttributeError: 'NoneType' object has no attribute 'WriteI2C'

    Part Number: ALP
    Other Parts Discussed in Thread: DS90UB9702-Q1EVM

    请问以上问题,我应该怎么办?感谢

  • DS90UB948-Q1: 如何将设置ds90ub983设置成测试模式去输出测试图像?

    Part Number: DS90UB948-Q1
    Other Parts Discussed in Thread: DS90UB983-Q1, ALP

    我们是一个车载项目,使用ds90ub983作为SER,使用DS90UB948作为DES。

    现在,我们需要在测试模式中设置关于ds90ub983-q1的寄存器,以显示DS90UB948中的测试图像。这是为了向客户展示它可以正常工作的。

    此外,我们的LCD尺寸为1920x720。

    以上。

  • DS90UB954-Q1EVM: 与SK-TDA4VM连接,在没有摄像头的情况下,有什么方法能够进行回环测试模拟图像传输

    Part Number: DS90UB954-Q1EVM
    Other Parts Discussed in Thread: SK-TDA4VM, TDA4VM, ALP, USB2ANY

    如题

    我们将解串器与SK-TDA4VM连接成功,但是由于sensor设备未到,请问TI有无提供某些方法模拟数据传输,从而验证数据通路(960<--->soc)的正确完整

1 2 3 4 5 »