This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1450: ISO1450BDWR 当D电平为1.8V时差分出来的Y信号没有发生电平变化,Z电平为3.3V 。Y的信号发生故障

Part Number: ISO1450

image.png    你好,当我使用ISO1450BDWR    给D发送一共电平为1.8V的逻辑电平时差分出来的Y信号电平未出现明显变化,在示波器上仅能看到400mV的微小电平一闪而过,Z电平能正常变为3.3V   。Y的信号发生故障 ,故障图像如上图所显示。当更换芯片为ISO1452BDWR 则,能看见  Y 和Z 的电平都能正常跳变成3.3V。我取消了R110 R94 R119 和ESD也是同样的故障。请问是器件使用方法不对?