This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1050: ISO1050 canH与canL之间加电容与不加电容的波形不一样

Part Number: ISO1050

你好! 

      ISO1050 CANH与CANL之间加电容与不加电容的波形不一样,请问一下有没有其他解决方案 ?

1、这一张是测试canH与canL上的波形,can线长35米,匹配电阻两端都是120Ω并在can线上。

2、这一张是我在ISO1050芯片的canH与canL引脚加1nF电容的,测试线上canH与canL上的波形,can线长35米,匹配电阻两端都是120Ω并在can线上。