Part Number: ISOW7841
你好
现在我再正规购买了 10片ISOW7841。
我们为客户购买了一盒,用其中5片,做了5组测试。
第一脚 ,VCC 接5V。外部电源。
测量Viso 脚,按数据手册,设置反馈,使Viso 输出约3.3V。但是,实际上测量Viso与GND2之间电压。
第一片,约1V。
第二片,约1.725V。
第三片,约4V。
第四片,约1.7V。
第五片,约1V。
这是为什么,是不是芯片里的DCDC转换有问题。
或者是在使用上注意的细节,没有注意到。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.