This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
ISOW1412 是RS-485/RS-422 收发器,隔离式CAN收发器建议您看下下面产品:
https://www.ti.com.cn/zh-cn/isolation/isolated-interfaces/can-transceivers/products.html
其中 价格比较便宜的 ISO1044 是 隔离式 CAN FD 收发器,Supports classic CAN up to 1 Mbps and FD (flexible data rate) up to 5 Mbps
ISO1044 的 TXD/RXD 需要接TXD/RXD CAN-FD 控制器,因为ISO1044 只是CAN 收发器,没有集成CAN控制器;
如果您的MCU没有TX/RX CAN-FD 控制器,您可以考虑再加一级CAN 控制器。
您可以考虑的整体方案是MCU的SPI -> TCAN4550(CAN控制器的功能) -> TXD/RXD -> ISO1044 -> CANbus. 因为 TCAN4550 具有一种模式,即您可以断开CAN TXD和RXD信号以与外部CAN收发器配合使用。具体见下面链接中的回复: