Part Number: ISOW1412
Other Parts Discussed in Thread: ISO1044, TCAN4550
1、项目需要 UART 转 CAN 通讯,带隔离,查到 ISOW1412 有 MCU TXD/RXD,不确定是否是 UART 的 TXD/RXD 还是 CAN 的,规格书里边并没有描述。
2、帮忙推荐 UART 转 CAN FD IC 或者 设计,最好 >=1Mbps。如果没有这么高的,也可以 500Kbps 。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
ISOW1412 是RS-485/RS-422 收发器,隔离式CAN收发器建议您看下下面产品:
https://www.ti.com.cn/zh-cn/isolation/isolated-interfaces/can-transceivers/products.html
其中 价格比较便宜的 ISO1044 是 隔离式 CAN FD 收发器,Supports classic CAN up to 1 Mbps and FD (flexible data rate) up to 5 Mbps
您可以考虑的整体方案是MCU的SPI -> TCAN4550(CAN控制器的功能) -> TXD/RXD -> ISO1044 -> CANbus. 因为 TCAN4550 具有一种模式,即您可以断开CAN TXD和RXD信号以与外部CAN收发器配合使用。具体见下面链接中的回复: