This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7710-Q1: 设计评估问题

Part Number: ISO7710-Q1

如上图,如果ISO7710FQDRQ1的1号脚不连接到电源,只有3号脚连接到电源,同时R1340电阻为300Ω,不知道这个应用是否可行。

  • 您好,

    引脚1和3在内部相互连接,因此命名相同。 断开其中一个不会影响设备工作。

    不知道您使用的VDD1电压是多少,如果是2.5V供电,工作速率100Mbps的话,将会在300Ω电阻上产生0.36V的压降,VDD1的供电电压将是2.14V,小于推荐的最小供电电压范围。总之,您要考虑串联电阻的压降对供电电压的影响,已经对VIL和VIH的影响。

  • 您好,

    目前供电是5V,但是可能会面临有个高达20V的尖峰无法消除,因此尝试增加了300Ω电阻尝试滤除尖峰,有几个问题如下,请帮忙解答

    1.串联300Ω电阻对毛刺尖峰下降的影响

    2.R1340电阻最优阻值如何选型

    3.取消1号引脚供电后的风险评估及可能的失效模式

    4.是否可以提供ISO7710FQDRQ1内部设计图

  • 1.串联300Ω电阻对毛刺尖峰下降的影响

    2.R1340电阻最优阻值如何选型

    加个大点的滤波电容效果怎样?或者考虑加TVS管或稳压管消除20V尖峰。

    3.取消1号引脚供电后的风险评估及可能的失效模式

    如上所述,引脚1和3在内部相互连接,因此命名相同。 断开其中一个不会影响设备工作。

    4.是否可以提供ISO7710FQDRQ1内部设计图

    很抱歉不可以分享内部设计图