如上图,如果ISO7710FQDRQ1的1号脚不连接到电源,只有3号脚连接到电源,同时R1340电阻为300Ω,不知道这个应用是否可行。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.串联300Ω电阻对毛刺尖峰下降的影响
2.R1340电阻最优阻值如何选型
加个大点的滤波电容效果怎样?或者考虑加TVS管或稳压管消除20V尖峰。
3.取消1号引脚供电后的风险评估及可能的失效模式
如上所述,引脚1和3在内部相互连接,因此命名相同。 断开其中一个不会影响设备工作。
4.是否可以提供ISO7710FQDRQ1内部设计图
很抱歉不可以分享内部设计图