This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1640: SIDE1有信号,SIDE2没有输出信号

Part Number: ISO1640


Hi,

我们在使用ISO1640做I2C隔离的过程中,信号没有通过隔离器。

下图为原理图部分:

下图为side1的输入信号:

很抱歉我没有保存下输出信号的图片了,输出始终保持高电平(副边的5V)。

已经验证过原副边供电正常,且更换过新的器件。

能否帮我检查一下原理图设计,分析一下可能的原因?

Best Regard

Zhuo