This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOUSB211: ISOUSB211识别问题

Part Number: ISOUSB211


您好:

我现在采用ISOUSB211进行USB隔离设计,遇到一个问题,经过集线器与PC连接时,可以识别USB设备,但直接与PC连接时,就不能识别设备,请问可能是什么原因导致的呢?

原理图如下

尝试了把C124和C77更换位10uF电容,D+/D-数据线串联22Ω/51Ω/100Ω电阻都没有解决问题,还有哪些方面可以考虑呢?

在PCB布线时,D+/D-特性阻抗是90Ω还是50Ω呢?