Part Number: ISOUSB211
您好:
我现在采用ISOUSB211进行USB隔离设计,遇到一个问题,经过集线器与PC连接时,可以识别USB设备,但直接与PC连接时,就不能识别设备,请问可能是什么原因导致的呢?
原理图如下
尝试了把C124和C77更换位10uF电容,D+/D-数据线串联22Ω/51Ω/100Ω电阻都没有解决问题,还有哪些方面可以考虑呢?
在PCB布线时,D+/D-特性阻抗是90Ω还是50Ω呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请参考ISOUSB211EVM的电路设计,其支持隔离USB OTG。
www.ti.com/.../ISOUSB211DPEVM
下面链接中的帖子提供了评估板的设计文件,请参考。
e2e.ti.com/.../isousb211dpevm-pcb-design-files