• ISO1042: ISO1042信号干扰问题

    Part Number: ISO1042

    请问下造成这种干扰的可能因素是什么?是否是VCC电压选择不当造成的,需要额外加滤波电容吗?谢谢

  • ISO1042-Q1: VCC1侧使用1.8V供电时无法通信

    Part Number: ISO1042-Q1
    Other Parts Discussed in Thread: ISO1042

    TI专家,您好。

    最近我在使用ISO1042QDWVQ1做can通信时,参考数据手册,为了能直接连到1.8V的FPGA,在VCC1侧使用了1.8供电。但是实际电路无法正常通信,收发都不行。在FPGA和iso1042之间加一级电平转换,将FPGA的1.8V信号转为3.3V,ISO1042的VCC1使用3.3V供电后,能够实现can通信。VCC1和VCC2是供地的,没有隔离…

  • ISO1050: ISO1050DUB损坏

    Part Number: ISO1050
    Other Parts Discussed in Thread: ISO1042, TVS1401

    现场多次出现ISO1050DUB收发器损坏,前端的TVS正常,原理图如下;能否帮忙分析一下可能的原因,谢谢。

  • ISO1042: CAN DC Bus Fault Protection Voltage: ±70 V

    Part Number: ISO1042

    规格书中的DC Bus Fault Protection Voltage: ±70 V,这具体的解释是什么?

  • ISO1042: Power supply application of VCC2 of ISO1042

    Part Number: ISO1042

    Dear Ti Expert,

    I would like to ask about ISO1042 IC applications. I have more than two devices using ISO1042.

    Can I supply multiple ISO1042's VCC2 using one power supply?

    I can't find information about the power supply application…

  • ISO1042: ISO1042

    Part Number: ISO1042

    Dear Ti Expert,

    I would like to ask about ISO1042 IC applications. I have more than two devices using ISO1042.

    Can I supply multiple ISO1042's VCC2 using one power supply?

    I can't find information about the power supply application…

  • ISO1042: ISO1042偶發性損壞可能的問題?

    Part Number: ISO1042

    您好,請問TI工程師 我有一款治具上有使用ISO1042,但是偶爾會發生燒毀的問題!上圖為我目前的電路架構...

    我想請問在什麼不當可能的情況下會造成ISO1042損壞,如:Vcc灌回去TX或RX之類的情況?

    謝謝!

  • ISO1042: ISO1042

    Part Number: ISO1042

    我们做X-ray测试,发现料号ISO1042DW现货照出来的内部结构和我们之前封样的库存内部不一样,现货有白色的点可以照穿,请问这种现象是属于正常现象吗?

  • ISO1042: 请问vcc1为5v,vcc2为3.3v,can收发器可以正常工作吗

    Part Number: ISO1042

    canl和canh是3.3v供电,能否转成5v供电的rx和tx呢,二者如果电压不同,会出现错误吗?

  • ISO1042: 请问GND2接到哪里,VCC1和VCC2可以用同一个5V供电吗?

    Part Number: ISO1042

    尊敬的TI工程师,

          您好!

    1.请问GND2需要引出来,和CAN总线上其他设备的CGND连到一起吗?

    2.我设计的电路板上的所有的地都是一个地,CGND2需要接电路板的地吗,我对于CGND2接到哪里很困惑。