This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC2T245: SN74AVC2T245,双路电压 电平转换芯片,在其中一路电压(VCCB或者VCCA)丢失后(电压为0),IO的状态如何变化?

Part Number: SN74AVC2T245
Other Parts Discussed in Thread: TXU0202

如上图,

1、如果其它条件不变,USB_VCCIO这路电压突然丢失(变为0V),那A1脚是什么状态(上图配置A1为输出状态 B1 to A1):

1)Hi-z(高阻态),电路失效;

2)1.8V ;

3)0V;

4)1.8V或者0V跳动,有驱动能力但输出状态未知;

2、USB_VCCIO电压长时间丢失(0V),VCC_MIO长时间为1.8V,这种情况下SN74AVC2T245芯片会有损坏风险吗?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好,

    如果 USB_VCCIO变为 0V),所有 I/O 都将阻抗直到 USB_VCCIO 再次如果 USB_VCCIO 长时间变为 0V没有设备损坏的风险

  • 感谢你的答复,还有一个问题是在很多应用中,譬如可插拔USB周围的电平转换电路,在USB线未插入的时候,USB_VCCIO这路电源是没有电的,我仔细想了一下,没有电(floating)和USB_VCCIO为0V可能还有些区别;

    1、在我的设计中,USB_VCCIO这路电源有一个3k的电阻接到地,所以没有电的时候其电压就是GND,所以我已经明白在此时所有IO都是HI-Z状态,满足了我的要求;

    2、但在很多场景里,USB_VCCIO要么是悬空没接,要么是接固定电压的;我想问的是USB_VCCIO没有电(floating)和USB_VCCIO为GND这两效果是一样的吗?USB_VCCIO没有电(floating)时所有IO也是HI-z状态吗?

  • 如果未连接USB_VCCIO设备,设备不会损坏,但 I/O 不会进入 Hi-Z 状态。

    如果您正在寻找当 VCC 等于0V 或浮动时强制 I/O 进入 Hi-Z 状态的器件,那么请查看TXU0202。