This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、要用CD74HC4046AM这款芯片只用芯片内部的比较器1和比较器2,3号脚和14号脚分别接入同频率的不同相位的方波,芯片2号脚能正常输出方波,比较器2输出的13号脚不能正常输出方波。有没有只针对这块芯片的只用比较器1和比较器2的电路推荐。
2、CD74HC4046AM芯片输出的是5V电平需要转成3.3V的电平接入到DSP的ECAP口,用SN74LVC245ADWR芯片这块电平转换芯片需要A口5V输入B口输出3.3那么1号脚要接高电平,这个高电平用5V接还是用3.3.接?’
您好,
1、您实测13号脚输出的波形是什么样的?它输出的波形不是方波,可参考数据手册Figure5 PC2out波形,如下截图:
2、SN74LVC245A输入电平电压与供电电压有关,如果VCC=3.3V,则高电平需2V ≤ VHI ≤VCC,因此需要接3.3V
SN74LVC245A是总线收发器,不是专用的电平转换芯片,因此不仅需注意前级输出是否满足它的要求,同时也需注意其输出的高低电平是否满足后级需求
1号脚DIR口要拉高不可以用5V拉高,因为SN74LVC245A输入电平电压与供电电压有关,其推荐的供电电压最大到3.6V,如果使用标准电压3.3V供电,则只能使用3.3V拉高
是的,VCC用3.3V的话B这里输出最大就是3.3V,但是请注意,看上面我在数据手册中的截图,SN74LVC245A输出高电平电压与输出的电流多少有关,最大输出电压应该是供电电压VCC
如果您需要推荐电平转换芯片,您可以告诉我通过信号的最大频率吗?需要几通道的?
您需要传输的信号频率不大,基本所有的电平转换芯片都可以满足要求,通道是4个的,可以进行5V转3.3V的看下SN74LV4T125、TXS0104E 、TXB0104 其输出电平是否与后级电路兼容