This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、要用CD74HC4046AM这款芯片只用芯片内部的比较器1和比较器2,3号脚和14号脚分别接入同频率的不同相位的方波,芯片2号脚能正常输出方波,比较器2输出的13号脚不能正常输出方波。有没有只针对这块芯片的只用比较器1和比较器2的电路推荐。
2、CD74HC4046AM芯片输出的是5V电平需要转成3.3V的电平接入到DSP的ECAP口,用SN74LVC245ADWR芯片这块电平转换芯片需要A口5V输入B口输出3.3那么1号脚要接高电平,这个高电平用5V接还是用3.3.接?’
您需要传输的信号频率不大,基本所有的电平转换芯片都可以满足要求,通道是4个的,可以进行5V转3.3V的看下SN74LV4T125、TXS0104E 、TXB0104 其输出电平是否与后级电路兼容