This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您的意思是TXS0102输出口出现震荡与上电的快慢有关是吗?那您在上电时,将OE拉低,待电源稳定后,再将OE拉高,看是否仍震荡?
是A1、A2口都震荡吗?
我想这可能与输入信号的速率慢有关,下面datasheet截图,要求A口和B口信号的上升和下降沿的速率最大为10 ns/V,如果边缘慢速可能会导致输出故障 ,即 在一次触发结束后,慢速输入可以再次将输出拉低。形成振荡。
您可以在上电时,用示波器实测TXS0102端口波形吗,看其上升和下降速率是否小于10 ns/V
10nS/V这个不是对通讯速率的要求,是对数字信号上升沿和下降沿的坡陡的要求。在正常通讯时(非上电掉电期间),您输入信号的上升和下降沿的速率满足这个Δt/ΔV要求吗,如果满足这个要求,可以通过控制OE来解决。如果没有控制OE的控制信号,可以在输入端加上拉以提供一个确定的电平状态,看是否可以解决问题。但是这样会对输出低电平有一定影响,即会使输出的VOL增加,具体查看:
https://www.ti.com/lit/an/scea054a/scea054a.pdf
LSF0102也是适用于开漏和推挽应用的转换器,可以看下。