Part Number: TXS0102
Other Parts Discussed in Thread: LSF0102


我们如上图使用了TXS0102,在测试时发现,快速的off/on电源后会在A2测到9.8MHz的波形。于是我将A2和B2的电阻断开,测试发现震荡波形是从TXS0102本身发出的。
于是我去掉了1.8V与OE之间的10k电阻。发振的再现率变低了,但是仍然存在。
请教是什么引起的发振,如何解决。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
10nS/V这个不是对通讯速率的要求,是对数字信号上升沿和下降沿的坡陡的要求。在正常通讯时(非上电掉电期间),您输入信号的上升和下降沿的速率满足这个Δt/ΔV要求吗,如果满足这个要求,可以通过控制OE来解决。如果没有控制OE的控制信号,可以在输入端加上拉以提供一个确定的电平状态,看是否可以解决问题。但是这样会对输出低电平有一定影响,即会使输出的VOL增加,具体查看:
https://www.ti.com/lit/an/scea054a/scea054a.pdf
LSF0102也是适用于开漏和推挽应用的转换器,可以看下。