This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CD74HC4046AM需要用到比较器1和比较器2,电路图设计是在芯片3号脚和14号脚直接接进同频率不同占空比的方波,16号脚接5V供电,8号脚接GND,比较器1输出对应的脚2和比较器2对应的脚13拉出来,这么设计能不能输出电压波形。
看CD74HC4046AM供电电压是2V-6V的那么芯片的16号引脚供电是不是能接3.3V然后输出脚2号和13号脚是不是可以直接进到28335的捕捉口。
您好,
1、您是不使用解调器和VCO是吗?这是可以的,INH管脚接高电平可以禁用VCO和解调器
2、 PCnOUT输出电平电压与接的电平类型有关,参看下面datasheet截图;
另外, PC2OUT输出是三态输出,存在高组态,需要您确认下28335对其信号的捕获是否有影响。
比较器电路建议仿真以验证;
不使用的管脚请查看以下建议连接:
e2e.ti.com/.../faq-how-do-i-terminate-any-unused-channels-of-a-logic-device
什么情况下输出高组态,请查看我上面附的截图Figure 5,和查看datasheet 中Phase Comparator 2 (PC2)部分