This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4046A: CD74HC4046AM只用比较器1和比较2

Part Number: CD74HC4046A


CD74HC4046AM需要用到比较器1和比较器2,电路图设计是在芯片3号脚和14号脚直接接进同频率不同占空比的方波,16号脚接5V供电,8号脚接GND,比较器1输出对应的脚2和比较器2对应的脚13拉出来,这么设计能不能输出电压波形。

CD74HC4046AM供电电压是2V-6V的那么芯片的16号引脚供电是不是能接3.3V然后输出脚2号和13号脚是不是可以直接进到28335的捕捉口。

  • Part Number: CD74HC4046A

    CD74HC4046AM 看芯片资料供电是2-6V,用的芯片是DSP28335,我是不是可以设计4046供电用3.3V然后比较器1和比较器2的输出直拉到DSP的捕捉口?

    CD74HC4046AM比较器1和比较器2的应用,3号脚和14号脚直接接方波信号,供电脚16用3.3V,8脚接gnd,2号脚和13号脚直接接到DSP的捕捉口ecap1和ecap2口,这么设计可行吗?

  • 您好,

    1、您是不使用解调器和VCO是吗?这是可以的,INH管脚接高电平可以禁用VCO和解调器

    2、 PCnOUT输出电平电压与接的电平类型有关,参看下面datasheet截图;

    另外, PC2OUT输出是三态输出,存在高组态,需要您确认下28335对其信号的捕获是否有影响。

  • 是的,我用不到解调器和VCO只用到比较器1和比较器2.

    图纸想直接这么设计。这里的Vin和Iin是我转换过来的一个交流电压通过和GND做了个比较输出3.3V的方波,可以行的通吗。还有这里比较器2的高阻态是什么情况下出现。

  • 比较器电路建议仿真以验证;

    不使用的管脚请查看以下建议连接:

    e2e.ti.com/.../faq-how-do-i-terminate-any-unused-channels-of-a-logic-device

    什么情况下输出高组态,请查看我上面附的截图Figure 5,和查看datasheet 中Phase Comparator 2 (PC2)部分