Part Number: LSF0102
双向电平转换芯片LSF0102实现网络MDC/MDIO电平转换,只能1对1么,
是否可以使用双向电平转换芯片LSF0102实现如下转换方式功能
连接方式1:

连接方式2:

连接方式3:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LSF0102
双向电平转换芯片LSF0102实现网络MDC/MDIO电平转换,只能1对1么,
是否可以使用双向电平转换芯片LSF0102实现如下转换方式功能
连接方式1:

连接方式2:

连接方式3:

您好,您的意思是,比如连接1,指的是芯片1和MDC/MDIO的接口进行切换,然后再使用LSF0102进行电平转换吗?
同样,连接3 也是,芯片1和MDC/MDIO,或者芯片3和MDC/MDIO 接口进行切换,再经过LSF0102进行电平转换吗?
芯片1、芯片2、芯片3都是PHY芯片,处理器通过MDIO接口访问这3个芯片,但是不同芯片的电平不一样,和处理器直接连接的芯片是1.8V电平,经过电平转换芯片的芯片是3.3V电平
您好,那不能满足您的要求,比如芯片2需要3.3V,那么LSF0102的VCCB需要接3.3V,同样如果芯片3需要5V,那么VCCB接5V,不能输出既可以是3.3V也可以是5V。
这样连接,需要考虑两个问题,一个是驱动能力,一个是阻抗匹配。
但是对于LSFxx的电平转换来说,是没有驱动能力的,它的驱动能力完全取决于外部上拉。
考虑到接多个外设,按照您的应用,处理器应该也是点对点通信,比如处理器只能和芯片2或者3通信,那么可以考虑加一个switch。